powered by CADENAS

Manual

Manual

2.2.5.  Move class

Via Move class you have the option of moving a specific directory or project within the entire directory structure. To do so, do the following:[7]

  1. Click on toolbar, Move class .

    -> The Move class dialog opens.

  2. Mark the Source class.

    Click on Move class -> Move... in the context menu of marked class.

  3. Mark the Target class.

    Click on Move class -> Set as target in the context menu of marked class.

    [Note] Note

    In the opened dialog window you can change the selection of source and target anytime with the above shown context menu commands.

  4. Confirm with Ok.

  5. Result:

    The "Head cap bolts" class has been moved under "Special sizes" class.



[7] The described way of proceeding gives you full control, because in all steps the dialog stays open and you can see changes in the fields at once.