Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
There are two different configuration options for importing STL files:
[STLIMPORT] OnVariant=0/1
If you decide on this option, set the value to '1' and OnClass to '0'.
Use this option, if there is an STL file for each row (article number).
Note | |
---|---|
In this case, the columns MATNR, CLASSNAME and STLFILE Fig. „filelist.txt“ are standard and must be filled out. Compare |
[STLIMPORT] OnClass=0/1
If you decide on this option, set the value to '1' and OnVariant to '0'.
Use this option, if there is an STL file for each class.
Note | |
---|---|
In this case, the columns CLASSNAME and STLFILE standard and must be filled in; the MATNR field must remain empty. |