powered by CADENAS

Manual

Manual

2.1.5.5.4. Add document link (green column)

Standard supplier catalogs can contain document links. These are displayed in a green additional column (compare Section 3.1.1.7.1.1, “ Determine characteristic in table view ” in PARTsolutions / PARTcommunity4Enterprise - User manual). Mostly documents in text, image or internet file formats are linked here.

As of V9.03 SP3 you can use this feature for catalogs, which have been created with the Classimporter.

In order for the document link column to be displayed, do the following:

  • Setting in attributedef.txt

    In the "ATUDF" column (attribute definition) set the value 'D'. Thereby a document link column is created.

    Possible values are:

    • A: Text

    • I: Integer

    • F: Floating

    • D: Document link

      If 'D' is set, then the creation of the "ATTRIBUTE_DOCLINK" column is necessary (see next item), in all other cases not.

    Set the text to be displayed (here in the example the term "Infotext") in the "ATBEZ_german" column (and accordingly in the languages to be translated, on this see Section 2.1.5.5.3.1, “Translatable text attributes”).

    "CLASSNAME";"ATTNAM";"ATUDF";"EINHE";"ANZDZ";"ATWITHLIST";"ATWITHRANGE";"ATBEZ_german";...
    "c_1734842242_0";"Idx";"I";"mm";"4";"";"";"Index";"Index";"";""
    "c_1734842242_0";"Doc";"D";"";"";"";"";"Infotext";"Infotext";"";""
    "c_1734842242_1";"Idx";"I";"mm";"4";"";"";"Index";"Index";"";""
    "c_1734842242_1";"Doc";"D";"";"";"";"";"Infotext";"Infotext";"";""
    "c_1734842242_2";"Idx";"I";"mm";"4";"";"";"Index";"Index";"";""
    "c_1734842242_2";"Doc";"D";"";"";"";"";"Infotext";"Infotext";"";""
    

  • Settings in attributedata.csv

    Create a column "ATTRIBUTE_DOCLINK". The values are links.

    "MATNR";"CLASSNAME";"ATTRIBUTE_NAME";"ATTRIBUTE_VALUE";"ATTRIBUTE_FL_VALUE";
    "ATTRIBUTE_FL_MAX_VALUE";"VALDESC_german";"VALDESC_english";"ATTRIBUTE_DOCLINK"
    "l_1734842242_0";"c_1734842242_0";"Idx";"";"0";"";"";"";""
    "l_1734842242_0";"c_1734842242_0";"Doc";"Link";"";"";"";"";"F:/Links/text_0.txt"
    "l_1734842242_1";"c_1734842242_0";"Idx";"";"1";"";"";"";""
    "l_1734842242_1";"c_1734842242_0";"Doc";"Link";"";"";"";"";"F:/Links/text_1.txt"
    "l_1734842242_2";"c_1734842242_0";"Idx";"";"2";"";"";"";""
    "l_1734842242_2";"c_1734842242_0";"Doc";"Link";"";"";"";"";"F:/Links/text_2.txt"

    [Note] Note

    The link should not reference CADENAS_DATA/23d-libs.