powered by CADENAS

Manual

Manual

3.1.7.6.7.  Define section cut...

In the 3D view, define a sectional cut with the desired offset to zero plane.

Call

Click on the respective button in the toolbar or alternatively on the command Define section cut... in the context menu of the 3D window.

Setting options

After calling the section cut a navigation cross with 6 arrows is displayed.

  • Choose a sectional plane by clicking on the respective arrow.

    -> The cut is adjusted at once.

  • Move the sectional plane with pressed mouse key or by entering the desired value in the input field or via arrow key in the input field.

  • When clicking on the button rotate cut rotation lines are displayed at the navigation cross.

    Click on the desired line and rotate the cut.

[Tip] Tip

At first push the navigation cross to the side and then perform cutting operations.