powered by CADENAS

Manual

Manual

3.1.11.9.  Status indicating bitmaps for table view (Status light)

Preferred parts can be tagged in many ways. Not only red-green display is possible, in fact any color or icon can be used.

Status icons can signalize an Export restriction or just have indication function.

Standard red-green display

Standard colors: Red/Green - Export possible: Yes/No

Standard colors: Red/Green - Export possible: Yes/No

Parts for which the status light is set to green may be exported to the CAD system. Parts for which the status light is set to red may not be exported to the CAD system.

Detailed information on how to define rules is found under Registerseite Allgemein.

Enhanced status icons

The standard red/green display can be enhanced, so that any amount of colors (icons) can be displayed.

In any case labeling facilitates controlled usage of parts.

A useful rule could be the following for example:

Dark green   =  Already used at all locations
Medium green =  Already used at two locations
Light green  =  Already used at one location
Yellow       =  Used at no location, but with ERP number
Red          =  Not according to any default

A color could be defined which signalizes whether a part is in stock. Each rule which can be deduced from table or project information is possible!

Status light with additional information characterStatus light, enhanced

Status light with additional information character

When moving your mouse over the status icon position (if highlighted), a tooltip shows up.

The status icons are also displayed in Vertical view type, in the list field of each variable.

Detailed information on how to define rules is found under Registerseite Anzeige.