powered by CADENAS

Manual

Manual

2.6.6.  Replace

The following describes how single parts from the standard and supplier part library can be replaced through alternatives.

  1. Mark the desired object in the CAD system.

    Figure exemplarily from Creo (in principle identical in all CADs)

    Figure exemplarily from Creo (in principle identical in all CADs)

  2. Click on the menu item Replace.

    -> The query dialog Choose procedure is displayed.

    • Replace selected instance

    • Replace all instances

      All parts and assemblies in an assembly are searched through, both up and down.[18]

    • Cancel

    The following options can possibly be enabled by specific config settings in addition.

    • Replace all inside this assembly without subassemblies

    • Replace in the current assembly and all subassemblies

  3. Click on the desired option.

    -> The query dialog Komponentenprojekt im PartDataManager öffnen? is displayed.

    Komponentenprojekt im PartDataManager öffnen?

    Komponentenprojekt im PartDataManager öffnen?

    Select Yes or No. In both cases the view switches to PARTdataManager. One time the project of the component to be replaced is opened, the other time not.

  4. Select the object to replace the original.

  5. Click on the button .

    -> The view returns to the CAD system and the part (or several) is replaced.



[18] Can be disabled via config key, because searching of all instances may last some time.