Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
In SolidWorks, NX and Solid Edge the Level of Detail can be selected directly in the CAD. So, if desired, the Level of Detail can be determined for the export.
Information about individual specification of the LOD (possibly different depending on special catalogs, directories and projects) can be found under Section 2.2.8.7, “ Block [LOD] - Level of Detail ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.
If no special defaults have been made in PARTdesigner, the calculation of a Level of Detail is automatically processed for each setting in PARTdataManager.
Note | |
---|---|
Varying from the automatism, in PARTdesigner, during modelling, features can be specified as "hidden" or "shown" for each Level of Detail. Information about creating individual feature displays can be found under Section 6.6.2.10, “ Level of Detail ” in eCATALOGsolutions Manual. |
The following image shows the corresponding dialog for switching between Levels of Detail, using the example SolidWorks.