Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
In the image below you can see that for the selected nominal diameter "12" there is a length for bolt "DIN 7968", which leads to a row with green status display.
Rows with nominal equal to "12" AND length "40" to "100" are not allowed for export according to the status light.[101]
If you absolutely want to use length "40", this would mean:
[101] Finally this depends on the specific export restriction. It is also possible that parts without ERP number may be exported as well. In this case the status light would be only a hint.