Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
With click on the button Edit custom variables the Custom variables dialog box opens.
Here you can define variables, which will be shown at each part in the report in addition.
You can define both ERP variables and variables from the characteristic attribute table.
At first click on in order to add a new line.
At first determine the variable type. With double-click on a line under Variable type the list field opens with the following options:
With double-click on a line under "Variable" a list field with the following input options opens:
Options for variable type "ERP":
The ERP variables from the table are read and displayed in the list field. Select one of the displayed variables or enter yourself a value.
Options for variable type "Table":
The variables of the characteristic attribute table are read and displayed in the list field. Select one of the displayed variables or enter yourself a value.
Enter a label in the input field. It will be displayed in the report later.
Optionally you can select a unit in the list field.
If the variable has no own unit, the selected unit is displayed.
If the variable has a unit, the value is converted - if needed. (The conversion is only possible for the type "Table".)
The diameter in the table is displayed in "inch". You have selected "mm" in the list field. -> The value is automatically converted from "inch" to "mm".