Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Follow the steps listed below to download a CAD model:
In the download area of CAD models, under Edit CAD formats -> Add CAD formats select the transfer mode download. Then determine one or several formats and click on . (For details see Section 4.8.2.1, “How can I select a CAD format? | How can I define the transfer mode into the CAD system? (Supplier portals)”.)
-> The view returns to the dialog area Generation options / Selected formats. Confirm your entries by clicking on .
In the dialog area for the CAD model selection click on .
-> The information dialog Generating CAD models opens.
As soon as the generation has completed, the CAD models can be downloaded in this window directly. For this click on Download.
If you close this window, further CAD models can be selected.
Furthermore all generated CAD models are listed in the download area.
-> At the transfer mode CAD models to download the link text will be Download.
After clicking on the link Info specific part information is displayed:
In order to import the models into the CAD system, do the following: