powered by CADENAS

Manual

Manual

3.1.12.5.4.2. Example 2 - Bolt selected

Usually the selection of the bolt should be the first setting (filtration) .

The following image shows the value range display, after the bolt "GOST 7795_70" was selected.

Bolt "GOST 7795_70" selected

Bolt "GOST 7795_70" selected

Green, red and orange values are shown.

  • Nominal 22 is green: This means that the selected project for this value has an ERP connection.

    Nominal 24 is red: This means that the selected project for this value does not have an ERP connection. AND it is not possible to ever reach a "green path" by changing the project selection.

    Nominal 30 is orange: This means that the selected project for this value does not have an ERP connection. BUT it is possible to reach a "green path" by changing the project selection.