powered by CADENAS

Manual

Manual

3.1.6.8.2. Docking window Use Cases (Online)

In the Part selection and in the Part view use cases from the knowledge database are displayed in an own docking Use Cases (Online).

Each use case is displayed exactly at that position (directory or project level) where it has been posted.

Visibility on/off

In the context menu of menus and toolbars you can find the item Use Cases (Online). Via checkbox you can set the visibility as desired.

With a click in the title and pressed mouse key you can move the docking (window) at the desired position. With a click on the pin you can enlarge the dialog. When you click on the pin in the opened state, then the dialog section is fixed.

When you select a directory or project which contains an use case, the number of use cases is displayed in red.

Post an use case yourself

You can also participate yourself and post use cases. As soon you have registered the respective section is displayed. In order to register click on the respective link below.