Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Within PARTdataManager you can transfer complete screw connections (blind hole or through-hole) to the CAD system.
With click on Connection the Connection section is opened or called in the foreground (if already used). Furthermore window positions are reset.
When you start the connections functionality via PARTsolutions menu in your CAD system and menu item command Insert Connection the part thickness is calculated and transferred to PARTsolutions.
Anytime you can switch between Search and Part Selection, Part view and Connection via the View toolbar.
In version 9 the former PARTconnection has been reworked in many ways. Especially the functionality has been integrated in PARTdataManager.
The Load bolted connection dialog box is opened in the foreground by default.
So you can easily load already saved preferred screw connections. The window shows the following categories:
Via Extended Settings the behavior can be changed. Other options are:
You are supported at the connection selection by a preview image in addition to the display of the single connection components.