Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The part variables can also be shown and operated in a list view in addition to the table view.
The list display contains the following columns:
Meaning | |
Several values available in list field / Changeable value: When you select a value in the list field, then automatically depending variables are changed as well. The following two possibilities can occur:
|
|
The value has been pinned by clicking on or or by direct selection.
|
|
By clic5king on this symbol the Enter value window opens. For value ranges (yellow and orange fields) you may make a selection here. |
The value can be changed via the list field (if possible at all).
By clicking on the value range selection dialog is opened. Here the variable value can be changed as well.
Example - Quick restriction to desired values:
Variable L can still be defined as desired. -> Now the filter symbol is displayed here too. -> The two DIN962 options flange and hole are now also pinned. |
|