powered by CADENAS

Manual

Manual

3.1.1.10.5.1. Create and edit ERP connections

You can apply complete connections in the link database.

Save connection

Proceed as follows:

  1. In the ERP toolbar, click on Add dataset to link database .[67]

    Add dataset to link database

    Add dataset to link database

  2. ->The dialog box Connection appears.

    Assign name for connections

    Assign name for connections

    Name of the new connection: In the input field, enter the name according to the example below and confirm with OK.

    Gruppe1/ISO 4162

    The directory structure is shown in the Load bolted connection dialog box under the Database item (see below).

  3. -> The new ident-no. window opens. The Standard name of the assembly is automatically compiled from the standard descriptions of the single parts and is already entered in the respective field.

    Define the ERPNo (automatically or manually depending on default) and Material and confirm with OK.

    Automatic assignment of standard description - select material manually

    Automatic assignment of standard description - select material manually

    -> Now the connection is saved in the link database.

Open connection

In order for a connection saved in the link database to be opened again, proceed as follows:

  1. Click on OpenOpen.

    -> The Load bolted connection dialog box opens.

    Open connection

    Open connection

    Under Database you can see all connections, which have been saved in the link database.[68]

    Furthermore you can see connections in the Load bolted connection dialog box, which have been saved without ERP connection [Own bolted connections (this user) and Predetermined bolted connections (all users)].

  2. Under Database select the desired connection and click on Open selection.

    -> The connection is loaded.

3.1.1.10.5.1.1. Save single part

You can also save single parts of a connection in the link database.

Proceed as follows:

  1. In the Connection section select a single part.

  2. Within the Connection dialog box click on Single part.

    Assign name for connection

    Assign name for connection

    -> The new ident-no. dialog box opens, just like in the Part view via the ERP toolbar -> Add dataset to link database .

  3. Determine ERPNo (automatically or manually depending on preselection) and Material and confirm with Ok.



[67] For which users the function is available, is controlled via the role authorization. Also compare Section 3.1.2.7, “PARTdataManager – ERP/PDM extensions ”.

[68] Preview images are not available.