Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The following 3D CAD formats and 3D system neutral formats are available:
For each format the available tabbed pages are listed. With click on the link you can reach the respective section with further information.
Views tabbed page
Filter (Geometry) tabbed page, Export options tabbed page -> Insertion position, Options
Views tabbed page, Export options tabbed page -> Insertion position, Options
Filter (Geometry) tabbed page, Export options tabbed page
Filter (Geometry) tabbed page, Export options tabbed page
Creo Elements/Direct (CoCreate Modeling)
Filter (Geometry) tabbed page, Export options tabbed page
Creo Parametric 1.0, 2.0, 3.0 each 32 or 64 bit
Filter (Geometry) tabbed page, Creo Parametric tabbed page
Views tabbed page
Filter tabbed page
Views tabbed page
Filter (Geometry) tabbed page, Export options tabbed page -> Insertion position, Options
Views tabbed page, Export options tabbed page -> Insertion position, Options
Filter (Geometry) tabbed page, Export options
For each format the available tabbed pages are listed. With click on the link you can reach the respective section with further information.
Filter (Geometry) tabbed page, Export options tabbed page
Filter (Geometry) tabbed page, Export options tabbed page
Export options -> Export accuracy, Cross-section tabbed page
Export options tabbed page-> Export accuracy, Cross-section tabbed page, Transformation tabbed page, Reduction tabbed page
Export options tabbed page-> Export accuracy, Cross-section tabbed page, Transformation tabbed page
Export options tabbed page -> Export accuracy, Cross-section tabbed page, Transformation tabbed page
Export options tabbed page -> Export accuracy tabbed page, Cross-section, Transformation tabbed page
|
|
On the Export options tabbed page you can determine the Insertion position. In the Options section you can find the following setting options: |
|
On the Export options tabbed page you can adjust the Export accuracy.
Select the desired accuracy in the list field:
The part is calculated with the set level of detail before the export.
The function is identic to the level of detail option in PARTdataManager, but here only temporarily for the export.
On the tabbed page Transformation, you can adjust the axis orientation and scaling for the exported part.
On the tabbed page Reduction, you can not only specify a certain number of triangles, but also the required result quality.
Default: Reduces to the predefined number of triangles. If the current number of triangles undershoots the predefined count, no reduction will be made.
Light: Light reduction. Great for a simple reduction of the face count of Parts. The topology will not be changed. Circles will be approximated by many faces.
Medium: Medium reduction. Great reduction of the face count of any Part. The topology will not be changed. Circles will be approximated by less faces.
Rough: Rough reduction. Great reduction of the face count of big or highly triangulated parts. Can destroy the topology of small parts and can lead to edged circles.
Some CAD systems import PARTsolutions parts with the help of macros:
CATIA V4 IUA Macro 3D (see Section 3.1.2.1.2.2.11.1, “CATIA Macro ”)
SolidDesigner Macro 3D (see Section 3.1.2.1.2.2.11.2, “SolidDesigner/OneSpace Modeling Macro ”)
SolidWorks Macro 3D (see Section 3.1.2.1.2.2.11.3, “SolidWorks Macro ”)
Macros record the individual steps that are taken during the creation of a geometry. With the help of this record, the geometry can then later be "reproduced" in the CAD system.
In other words, the imported files are available without the usual connected information (dimensioning, part descriptions, etc.). In addition, no thread display is possible for example.
Note | |
---|---|
For connections, the export via macros is unreasonable, since the important connection information (create with borings, etc.) cannot be exported along with them. |