Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The following 3D transfer formats are available:
The file format *.ps3 on the one hand is the standard format, in which parts, assemblies, etc. are exported from PARTdataManager and with the help of an interface transferred to the respective CAD system. On the other hand files in this format can first be saved at any location and then imported to specific CAD systems.
The following 2D transfer formats are available:
After click on the desired format the dialog box Export using PS2-V1/2 2D format opens.
The following options are available:
Shortened view: When you want to export the shortened view, then activate the checkbox.
You can find detailed information on this under Section 3.1.1.11.3.1.4, “ Alternative 2D size Optimize drawing view on paper size / ”.
Source: In the list field there are two options:
At the desired views activate the checkbox.
Views: Detailed information on the individual views can be found under Section 3.1.1.11.3.1, “ "2D view" dialog box ”.
The options are only then active, when under Source the option Selected views is selected.
Via browse button choose the Destination file, where you want to save the part / assembly.