powered by CADENAS

Manual

Manual

3.1.1.6.4.7.  Search for unmachined parts

Function description

The Search for unmachined parts detects fitting unmachined parts for the production of finished parts or finished parts which can be produced from a certain unmachined part.

Example:

An engineer is looking for a special flange. Then he wants to search for already existing unmachined parts, from which the flange can be produced, in order to avoid the redundant creation of a new unmachined part (material master). This process is very time consuming, because the parts have to be overlaid in the CAD one after another

With Search for unmachined parts this can be solved much quicker.

The search detects, whether a part is completely contained in another part: The finished part has to be smaller than the unmachined part, so that it can be produced by removing wasted material. As soon as the extensions of the finished part exceed the ones of the unmachined part only at a certain point, it cannot be used at all or at least badly.

The search calculates the volume of the material to remove (waste). The less material to remove, the higher the ranking in the result list, because this criterion is determining for the manufacturing costs.

Call:

When searching with one single part call the Search for unmachined parts from the standard search methods area. The advantage is that it can be combined with other methods such as Full-text search [41], Variables search or Topology search). The combination with Geometric search (3D), Sketch search (2D) and Color search is not possible. When searching with multiple search parts further on use the "Search for unmachined parts" via Purchineering functionality. On this see Section 3.1.2.3.3, “ Search for unmachined parts ”.

In this example the "Search for unmachined parts" has been combined with the Full-text search.

In this example the "Search for unmachined parts" has been combined with the Full-text search.

Settings dialog:

When clicking on the icon Search for unmachined parts the same-named dialog box opens.

  • History:

    On the left side under History select the desired search part.

    • Tabbed page Projects

      If the needed search part is not yet displayed you have to load it in the Part view first.

    • Tabbed page 3D files

      You can use any 3D file as search part:

      • When you click on Geometry from CAD the part or assembly selected in the CAD system is loaded into the dialog.

      • When you click on Load geometry, an Explorer window opens where you can browse to the desired geometry.

  • Settings:

    • Under Settings, in the list field, select ...

      • Search unmachined parts for finished part

      • Search finished parts for unmachined part

    • Accepted error in finished part

      The error is caused by missing material at the unmachined part.

    • Maximum waste in unmachined part

      The maximum waste defines how much material may be removed from the unmachined part.

    • Resolution: (16 | 32 | 64 | 128)

      The resolution controls the search quality. When choosing a higher resolution more details are gathered, however, the search lasts a little bit longer.

Result:

  • In the column Search for unmachined parts, Protrusion and Waste are displayed, both in absolute and percentual values.

    Protrusion: Missing volume in the unmachined part

    Waste: Waste volume of the unmachined part

  • With mouseover at the preview image, a 3D-preview is displayed. A Protrusion is marked with red color.

    Mouseover shows a 3D preview

    Mouseover shows a 3D preview

  • When clicking on the button Compare unmachined part with finished part the parts are opened in the Part comparison. A Protrusion is marked in red color. In the part comparison you have many different 3D comparison methods available. Details on this are found under Section 3.1.1.6.10.3, “ 3D comparison ”.



[41] additional information such as material for example