Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
By default, only the Full-text search is fully visible. The other search methods are hidden, however, can be called up anytime.
You can open or hide the dialog area of search methods when clicking on the arrow icons . Default is hidden state.
In the hidden state just as well, you can access all search methods.Simply click on the green Plus button . Used methods are displayed with checkbox (enable/disable) and icon. When clicking on the icon the respective dialog box opens.
In the hidden state you can use Cloud Navigator or Cloud Map search as well.
Therefor click on the small arrow in the button .
When opening the area of search methods you can see the concrete search parameters in addition and beside the start buttons the button for .
The following depictions show the area of search methods in opened state.