powered by CADENAS

Manual

Manual

2.6.12.  Settings

As of PARTsolutions Version 9, all settings for CAD systems are based on configuration files that are managed via the PARTadmin module.

By clicking on Settings, PARTadmin opens automatically.

PARTsolutions
Insert 3D
Seamless
Replace
Extras
Execute Geometric Search
Insert Connection
User library
Settings
Info

For each CAD system there are two setting areas:

  • CAD integration -> Common

    [The related configuration file is stored under $CADENAS_SETUP -> ifacecommon.cfg (usually only accessible administratively)]

  • CAD integration -> Specific CAD name

    [The related configuration file is stored under $CADENAS_SETUP -> if"abbreviation cad name".cfg (usually only accessible administratively)]

CAD configuration via PARTadmin exemplarily with the selection "Inventor"

CAD configuration via PARTadmin exemplarily with the selection "Inventor"

Detailed information about administrating configuration files can be found under Chapter 2, PARTsolutions - CAD Integration - Administration in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.