powered by CADENAS

Manual

Manual

3.1.2.3.1.5. "Find suppliers" report
  1. In the index tree select a directory or project.

    [Note] Note

    The generation time both depends on the size of the own parts pool to be searched and on the amount of supplier catalogs (directories) to be searched. In order to get a quick overview on the functionality best select a single own part and 2 or 3 supplier catalogs to be searched.

  2. Under Extras menu -> Purchineering -> Find suppliers call up the command Create report....

  3. -> The settings dialog opens.

    You can search for suppliers via:

    • Geometrical similarity:

      Searching for geometrical similarity is the standard case at all reports. At the supplier search a textual search is possible instead or in addition. See next checkbox.

    • Norm numbers:

      A textual search in all available part information concerning reference statements to standard parts is performed.

    Under Threshold in % choose 70 for example.

    In the search in following directories section select the desired catalogs, directories or subdirectories.

    Settings for "Find suppliers"

    Settings for "Find suppliers"

    Details on the settings dialog are found under Section 3.1.2.3.1.9, “Setting options for "Make or Buy", "Find suppliers", "Cost mockup"”.

    Confirm with OK.

  4. Result:

    Under Overview at first you see the Catalog overview.

    Catalog overview: You can see the found parts at each catalog.

    Catalog overview: You can see the found parts at each catalog.

    Click on Part overview.

    In the part overview you see a matrix. It shows, which concrete parts have been found in which catalog.

    Example

    Example

    Click on the button Go to search results.

    You receive a listing of all matching comparison parts in the respective catalog.

    Example

    Example

    Depending on whether you have searched for geometrical similarity or for reference statements in the settings dialog or both, now you can see information on norm number and/or Geom. Search at the found parts.

    A description on the single icons is found under Section 3.1.2.3.1.10, “Icons in "Make or Buy", "Find suppliers", "Cost mockup"”.

    A description on the single buttons is found under Section 3.1.2.3.1.11, “Buttons ”.

[Note] Note

Selection dialog for non-unique import formats:

If there are import formats in the chosen directory, which cannot be clearly assigned, then a selection dialog box is displayed.

At the correct format, activate the checkbox and confirm with OK.