powered by CADENAS

Manual

Manual

2.6.2.  Insert 3D from the Standard and supplier parts library

The following describes how you can insert single 3D parts from the Standard and supplier parts library into your 3D CAD system.

[Note] Note

The default procedure is described.

For some CAD systems you can find further information in the CAD specific chapter.

  1. In the PARTsolutions menu click on Insert 3D.

    -> The display switches to PARTdataManager.

PARTsolutions
Insert 3D
Seamless
Replace
Extras
Execute Geometric Search
Insert Connection
User library
Settings
Info

  1. In the Part selection choose the desired parts.[7]

    PARTdataManager - Part selection

    PARTdataManager - Part selection

  2. Determine the desired characteristic in the Part view .

    PARTdataManager - Part view

    PARTdataManager - Part view

  3. Click on .[8]-> The display switches back to the CAD system.

  4. The PARTsolutions placement dialog appears.

    [Note] Note

    The placement dialog box is available for the interfaces of Inventor, Pro/Engineer | Creo Elements/Pro | Creo Parametric, Solid Edge, SolidWorks and NX. In the other CAD systems the placement is performed by using the default methods.

    1. Select method

    1. Select method

    The placement methods available in a certain case depend on the part type.

    Not all parts in the standard catalog have all the attributes needed for additional PARTsolutions intelligent placement methods. The method "Default placement" is always available. Currently the CAD interfaces enable the additional intelligent placement methods for rotationally symmetric parts such as bolts, nuts, rings and bearings for example.

    The following figure gives an overview about the parts which enable intelligent placement in addition.

    Select a placement method:

    1. CAD system (Default CAD placement method)

      This placement method is always available.

    2. In Cylinder (PARTsolutions placement method)

      e.g. for placement of bolts, but also for bearing on shafts

    3. On surface (PARTsolutions placement method)

    4. Touching Surfaces (PARTsolutions placement method)

      e.g. for placement of countersunk screws

    [Note] Note

    For not available placement methods the respective button is deactivated. Especially at connection components there are several methods available.

    1. Select method: before selection

    1. Select method: before selection

    1. Select method: after selection with the checkbox "Repeating"

    1. Select method: after selection with the checkbox "Repeating"

    The activation of the Repeating checkbox enables the repeated placement in the CAD without having to use the Repeat [9] button.



[7] A detailed description of PARTdataManager can be found under Section 3.1, “ PARTdataManager ”.

[8] You can also export the part via "Export in file". More detailed information can be found under Section 3.1.2.1.2, “ Export to CAD systems without PARTsolutions interface - Export in file ”.

[9] At certain CAD systems the function is available for all placement methods, at others only for the Standard CAD placement method. If the function is not available, then the checkbox is grayed out.