powered by CADENAS

Manual

Manual

3.1.19.2.6.5.  Physical properties of the part

  • Via this command you can see the physical properties of the respective part and calculate volume and center of gravity.

  • Via the Surface, Volume, Weight and Center of gravity list fields you can set the respectively desired Unit.

  • Material:

    • Either use the list field above

      or

    • select the checkbox Use for all single parts and assign the material for each part separately in the respective list fields.

Volume and center of gravity

Volume and center of gravity

[Note] Note

In the row of the single parts there is no multiplication with the amount of parts. The final result regards the amount.