Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
In the Details mode you receive more information such as Name, Description, Version, Unit, End date, etc. in a table view.
To navigate in the depths, double-click on a row.
Results after double-clicking:
The selected directory shows up in the breadcrumbs row. (See Section 3.1.6.4.11.7, “ Navigation via navigation path (breadcrumbs) ”)
Under Details now the elements of the next lower level are displayed.
You go one step back each time you click on the "Back" button.
On the left in the tree the respective level is also selected.
Especially when Preview and Company logo are set on "small" it is helpful to move the mouse over the preview images in order to display the 3D Tooltip.
The 3D Tooltip is scalable and animated. In the down right corner you can find a drag point to draw up the size. The extensions of X, Y and Z axis are automatically displayed.
Whether the 3D Tooltip (size small, medium, large) or a Preview image shall be used, you can set in the Extras menu under Preferences... -> Part selection -> 3D Tooltip:
Under PARTdataManager -> Extras menu -> Preferences... -> Part selection -> Show tooltip with previews you can switch on and off the Preview image.
Order and visibility of columns
You can set the order and visibility of columns. In the dialog box that shows up, you can activate/deactivate and move the desired columns. |
|
Via clicking on a column header, you can sort the rows depending on the values of the desired column.
If you use ERP integration, then you can sort via the red-green folder characteristic in addition.