powered by CADENAS

Manual

Manual

3.2.6.1.  Menu item "Order of columns"

The columns themselves are ordered as set under Bill of material menu -> Order of columns (see figure).

In this menu, you can move the relevant marked column by Drag & Drop or using the arrow buttons. The topmost position in the list corresponds to the left-hand column of the Table view.

If you want to hide a Column in the Table view, simply remove the respective checkmarks.

Via use as standard you can set whether the currently set order and selection for this form type (e.g. "Neutral") should be set as a presetting for files applied in the future.

[Note] Note

The total price for part lists with more than one total price row, is usually automatically calculated at the lower end of the table. This is only possible however if the price is entered in all total price rows.