powered by CADENAS

Manual

Manual

3.1.6.2.1.  Custom selection...

You have the opportunity to use and save your own search templates for the Keyword search so these can be immediately available to you at a later date.

In addition you can define a Default selection, which is automatically selected in the list field of the Keyword search when PARTdataManager is launched.

Keyword search with user-defined templates

Keyword search with user-defined templates

  • Create and save search template

    1. Under Search in select the Custom selection... list item.

      Selection: Custom selection...

      Selection: Custom selection...

      -> The Search path selection window opens.

      Search path selection

      Search path selection

    2. In the left dialog section Current selection activate the desired directories for the keyword search by activating the checkbox.

      [Tip] Tip

      To be sure that there are not any "old" selections anywhere click on Reset at the beginning.

    3. Under Template name enter a name and then click on Save. Alternatively you can use the return button as well.

      -> The template is now displayed under User defined templates.

      [Tip] Tip

      When you move the mouse over a user defined template then the selection related to the template is displayed.

      [Note] Note

      You may optionally define a Default selection, which is automatically selected in the list field of the Keyword search when PARTdataManager is launched.

      Therefor select the desired template and check Default selection.

    4. Close the dialog via Ok. Alternatively you can use the return button as well.

    5. Start the user-defined search via the Start search button.

    [Note] Note

    You can now open the saved search templates at any time under your name see below).

    • Ok

      ... closes the window and takes over the current selection into the keyword search. Alternatively you can use the return button as well.

      Exemplary selection "Würth"

      Exemplary selection "Würth"

      [Note] Note

      With Ok the current selection is used for a onetime search without saving it.

    • Reset

      ...deletes the current selection.

    • With Close the dialog is closed without saving any changes.

  • Modify saved search template

    In the list field (open with arrow key) click on Custom selection... in order to open the Search path selection window.

    Select a template in the right section User defined templates and click on Activate template.

    -> The corresponding selections are now displayed in the left main window Current selection again. Possibly modify these and save the selection again as a template.

    With Delete you can remove saved templates.

  • Use templates

    Already saved templates are displayed in the list field under the separator and can thus be directly selected.

    Saved templates / Default template

    Saved templates / Default template