Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The standard toolbar contains the following icons:
After activating via the buttons, only those rows which have an entry in a defined column will be displayed. (Often this is the column for the article number.)
Under Extras menu -> Settings... -> Table -> Variable for preferred rows you can determine the variable for preferred rows (without ERP connection).
Via ERP integration you can define the preferred row via role rights. See Registerseite Allgemein.
|
See Section 3.1.7.1, “ Determine characteristic in "Table" view ”.
This command opens the module PARTadmin. In order to update or install catalogs you need write permission. For missing write permission you will receive a corresponding message.
See under Section 1.3.3.1, “ Catalog update Online ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.
With PARTsolutions Version 9 all standard parts were changed to DIN 962. This controls how screws and nuts can be adjusted in special cases through additional forms and models.
Whether you would like the DIN962 options to be displayed in the table and list view can be decided by clicking on the respective button in the button bar.
Detailed information about configuration can be found under Section 1.7.5.7, “ din962_global.cfg - Variants in screws and nuts (DIN 962) ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.
Show/hide parts that should be avoided
In the DIN, EN and ISO datasheets (as well as other country standards) specific sizes are often considered unusable. The part distinction is carried out administratively.[119]
In the Assistant dialog box, the respective form is being loaded.
ere you can wish for preferred catalogs from manufacturers.
In order to offer you the biggest selection of suppliers, we are continuously trying to add more to our multitude of supplier catalogs. CADENAS is working at its highest capacity to make all suppliers with electronic product catalogs available.
Please support us in this matter and let us know your favorite manufacturer and/or let us know which manufacturers we do not have on our preferred list.
In the Assistant dialog window you will receive information about the new PARTsolutions Version 9.
For every part sketches and pictures can be displayed in order to show the exact position in the stock and rack.
By clicking on the icon storage area these are displayed in the Assistant.
[119] Detailed information about configuration can be found under Section 1.7.3.1, “ avoid_parts.cfg ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.