Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Using an example, the following shows how you can work with templates in the PARTdataManager.
In contrast to the configuration, the template assembly (file format *.sbl) completely or at least partially has automatic assembly. In the Assembly the Start element and the corresponding assembly components show up immediately (see Fig. „Templates with complete self-assembly“). |
|
Templates with complete self-assembly configure themselves 100% alone.
There are no more free (green) connection points. All connection points are displayed in black font.
Single elements can be removed or (if possible) replaced by alternative characteristics.
During a row change the template reassembles itself completely again.
Templates with partial self-assembly independently assemble themselves with a certain basic structure. Some Connection points are still open (green) and can be filled with preassigned elements. This template variant is a mixture between configuration and "full-template". It can also be changed and/or reduced.
Note | |
---|---|
The example can be found in the training catalog under "building blocks/building blocks - car". |
Fixed template: This assembles itself 100% automatically, it may however - in contrast to the other template types - neither be changed nor reduced. (See also Section 3.1.15.7, “Saving templates ”)