Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
By default, only the Full-text search is fully visible. The other search methods are hidden . You can open the area anytime to add other search methods or alternatively use them.
In the input field, enter a search term and click on .
Note | |
---|---|
You can combine textual and numerical terms. Both the table (ERP columns and characteristic attributes) and topological values are searched. |
Beside the Full-text search some other search methods which can be combined [40] are available in addition:[41]
For details please see Section 3.1.6.4.1, “When to take which search method?”.
Beside or instead of the full-text search other search methods can be used.
Open the area of search methods with the arrow key .
-> Then you will see a listing of all search methods.
Click on the link of the desired search method.
-> The respective settings dialog opens. After committing the settings the search method is displayed below the Full-text search with checkbox and "Remove" button . Furthermore you can see used setting parameters beside the search method.
In this exemplary figure all search methods have already been used and so are listed. Full-text search and Topology search search are activated and are used for the next search run.
Click on the "Remove" button .
In order to add a search method click on the green plus button and then on the desired method.
-> The respective settings dialog opens. Once committing the settings the respective icon of the selected method is displayed with activated checkbox.
Beside using the search functions, of course you can manually search the directory structure.
For example, on the tabbed page Part selection, select the subitem Catalogs or Classifications and search the respective directory structure for the desired component.
Detailed information on the single subitems (Catalogs | Classifications | Favorites | History | Document scan) can be found under Section 3.1.6.4.11, “ Part selection via index tree ”.
[40] only Sketch search (2D) and Geometric Search (3D) not together
[41] Full-text search and Variables search are always available by default. For all other search methods the license "CNS200x*PSADDONS*COMPLEXSEARCH" is required.
Information on how to check whether a certain license is available can be found under Section 6.5.1, “ License information ”.