powered by CADENAS

Manual

Manual

2.5.4.2.6. Physical properties from PARTsolutions

If on the side of PARTsolutions the physical properties are set in the CNS classification, then these are also transferred to the CAD system during the export.

In PARTdataManager the attributes of the CNS classification are displayed under index tree, context menu of a part, menu item Part information.

On the side of CoCreate only the physical property "density" is overtaken. Mass and volume are not overtaken.

Density (Part, ModelData)

Density (Part, InstanceData)

Density (Asm, ModelData)

Density (Asm, InstanceData)