Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The Full-text search is useful ...
...as standard search for standard and supplier catalogs
Search for names and dimensions, technical data (combination of text and number), which is included in the characteristic attribute table, classification, standard name, standard number, standard text and names of directories.
Hexagon bolt M10x50
Hexagon bolt 10 50
... when searching for topological measures of length
266 147 12
... at parts, which provide additional information from ERP/PDM system, e.g. material, surface, mechanical resilience, price, storage, etc.
... at parts, which cannot be described by geometry, parts without geometry, glues, oils, electromagnetic parts, all parts, where the outer form is irrelevant
For details please see Section 3.1.6.4.2, “ Full-text search ”.
The Variables search dialog box shows ERP variables by default, is thus advisable if you want to search for material, surface, storage, etc.
In addition, classified variables such as order number for example are displayed globally at each directory level.
Furthermore the common variables of the directory level selected on the left are displayed (under Search in, select the currently selected directory).
For each variable you can find mathematical operators:
= | equal |
<> | unequal |
<= | less than or equal to |
>= | greater than or equal to |
< | less |
> | greater |
x-y | from - to |
For details please see Section 3.1.6.4.3, “ Variables search ”.
The Geometric search (3D) is used based on a reference part
The Geometric search (3D) can be used ...
... at missing textual information or classification (especially company parts)
... if no adequate search term is known (possibly little expert knowledge)
... during modelling in order to avoid the creation of duplicates
... to compare supplier and company parts
Comparison of | Benefit | |
Company part | Company part | |
Company part | Supplier part | |
Supplier part | Supplier part |
The Geometric search (3D) provides a result list with percentual similarities
For details please see Section 3.1.6.4.4, “ Geometric search (3D) ”.
Supposed there is no reference part available for a "Geometric search", but you have a clear picture, then use the Sketch search (2D). Make a sketch or import one.
For details please see Section 3.1.6.4.5, “ Sketch search (2D) ”.
If the catalog supplier used colors then you can use the Color search in combination with other methods.
For details please see Section 3.1.6.4.6, “ Color search ”.
The Search for unmachined parts detects fitting unmachined parts for the production of finished parts or finished parts which can be produced from a certain unmachined part.
Example finished part from unmachined part: The search detects, whether a part is completely contained in another part: The finished part has to be smaller than the unmachined part, so that it can be produced by removing wasted material.
The search calculates the volume of the material to remove (waste).
For details please see Section 3.1.6.4.7, “ Search for unmachined parts ”.
With the Partial search you can search for certain features, patterns and arrangements in parts (assemblies), not for parts itself.
In the 3D view, select the desired features.
For details please see Section 3.1.6.4.8, “ Partial search ”.
Company parts from semi-finished products can be found very simple with the Classification 2.0 search.
No reference part available -> specify reference part with a filter assistant on the base of templates -> perform search
Base templates can be enhanced by customer-specific templates.
For details please see Section 3.1.6.4.9, “ Classification 2.0 search ”.
If there is no reference part available for the "Geometric Search (3D)", you can use the Topology search as an alternative as well.
Using the Topology search makes sense for parts which are described by their shape, but rather by specific features. An angle for example is a sheet of metal curved at a right angle, however the number, size and arrangement of its boreholes is very characterising.
Search for special topological attributes, which are characteristic for the desired part (within large assemblies as well):
For details please see Section 3.1.6.4.10, “ Topology search ”.