powered by CADENAS

Manual

Manual

3.1.6.4.2.4. What is searched?

The following data are part of the index. Thus, for those it can be searched in all languages:

  • Project

    • Path

    • NT

    • NN

    • Date

    • Catalog name

  • Table (+ERP)

    • NB

    • Fixed numerical values

    • Fixed textual values

    • Order number (defined by CNSORDERNO)

    • Value range variables with fixed values (no value range)

  • Classifications

    • EClass IDs or class description

    • Class attributes

  • Topological values

    [Note] Note

    Searched are measures of length. If you want to query specific topological characteristics use the Topology search.

    The additional searching for topological values especially affects own part catalogs, because here characteristic values are not necessarily found in the table.

Examples:

  • Topological information is displayed in its own docking window Topology information.

    The following figure shows an example where the textual search term "Tischplatte" is found in the table, however, the numerical value in the topological information.

  • The Project path is displayed on the tabbed page Search results, on project level, in the column Summary.

    When searching in another language than the set one (in the next figure exemplarily "schraube") you can see in the pop-up window under Hits where this is based on [NB (standard name), path and description].

  • In the following a search with "head cap bolt ISO" is conducted.

    The respective terms are marked on the tabbed page Search results:

    On project level: In Standard number (NN), Standard text (NT) and Project path

    On line level: In Standard number (NN), Standard text (NT) and Standard name (NB)

  • Hits based on table values are marked in yellow on the tabbed page Search results as well. In the following example a search for "hexagon bolt D=10 L=50" has been performed.