powered by CADENAS

Manual

Manual

2.3.4.1.8.  Key "Material" - Material mapping

If this key is set, the material should be applied with all physical properties.

The material name must be identical to one of the names in the material list (iProperties -> Physical tab -> Material)

Per default the value of this key is a complex vbs expression. It may be adjusted as desired.

Default:

Material=?context.TranslateStringInGlobalOptionArray(MATMAP,,_FORMAT_0(<CLASSPROP
 (cns,CNSPHYPROP,CNSMAT)>).value()) 

Further variants of values:

Material=?_FORMAT_0("<ATTR(MATERIAL)>").value()

May be combined with material mapping (internal PARTsolutions material name : CAD-System material name).

Material mapping is used in order to map the internal PARTsolutions material name onto the CAD system material name.

[Note] Note

The untranslated name of the material is transferred; in other words the same one for all languages.

Per default the material name is taken from the CNS classification. (Where the CNS classification gets the material name from is set under

C:\ProgramData\cadenas\partsolutions\setup -> configuration file partsol.cfg -> Block VARTOCLASSMAPPING. Per default the table column "MAT_NAME" is set.)

The determined name is then mapped along with the material table under block MatMap to the CAD system material names.

The following shows the [MatMap] block relevant for material mapping:

[MatMap]
Copper=Kupfer
Aluminum-6061-AHC=Aluminum-6061-AHC
Titanium=Titan
ABS Plastic=ABS PlastiK
Gold=Gold
Lead=Blei
Silver=Silber