powered by CADENAS

Manual

Manual

1.8.4.14.  "Statistic" tabbed page

On the Statistic tabbed page there are different methods available for statistic evaluation.

Example: Rejections by product

Example: Rejections by product

The procedure as overview

  1. Select a statistic type:

    • Usage by product

    • Activity per product

    • Activity per user

    • Activity per host

    • Rejections by product

    • Rejections by user

    • Rejections by computer

    • Usage by product

    -> On the right side diagram and table are displayed.

    [Note] Note

    If there is no display, then too strong restrictions have been made.

    Change settings in the dialog area Limits: Possibly Start date and End date or open the list fields of Products, User, Computer and clear the checkboxes.

    Now a diagram display should happen.

  2. The column display below the diagram depends on the selected type of statistic.

    You can show/hide columns in the dialog area Columns.

  3. Adjust the settings in the dialog area Restrict.

The single dialog areas and buttons

  • Selected statistic

    • Usage by product

      The statistic Usage by product lists the maximally available and used Floating licenses for all products within the defined period of time. If the number of In use (floating) licenses is very close to the number of available licenses, then you should consider the increase of capacity, even if there were no rejections yet. Also see the statistic types Rejections by product, Rejections by user and Rejections by computer.

      This type of statistic is especially suitable for analyses over a longer period (month, year).

      Available:

      All issued Floating licenses.

      In use (floating):

      Under In use (floating) the highest value ever occurred is displayed.

      In use (reserved):

      Reserved licenses are a subset of the In use (floating) licenses.

      • On the Checkouts tabbed page you can administratively determine, whether users are allowed to checkout Floating licenses. Detailed information on this is found under Section 1.8.4.8, “ "Checkouts" tabbed page ”.

      • The checkout happens in the respective module under ? menu -> Licenses (F9) -> Checkout tabbed page. See Section 5.5.1.5, “"Checkout" tabbed page”.

        Thereby the amount of available Floating licenses is reduced for the before defined checkout period.

        So a Floating license can be reserved for a certain time, for a journey for example.

      Used (sum): Is according to In use (floating).

    • Activity per product

      This statistic type is especially suitable for shorter periods of time, let's say 7:00 to 12:00 of a certain day. You can recognize the level of fluctuation, in relation to a certain product. High fluctuation confirms, that your decision for Floating licenses is correct.

      License pulls and Shares are counting events in a certain time period. If the analysis period is unfavorably chosen (8:00 to 12:00 for example), while start of work is at 7:00 (now the licenses are pulled), the releases can be higher than the license pulls.

      License pulls:

      Single events of license pulls are counted.

      Shares:

      Single events of license releases are counted.

      Rejections:

      Rejections can only occur, when there is no license available anymore at the moment of request.

      If there are rejections, then the amount of Floating licenses should be increased.

    • Activity per user

      Analysis of user behavior. Many rejections? High fluctuation at license pulls and releases?

      License pulls:

      Single events of license pulls are counted.

      Shares:

      Single events of license releases are counted.

      Rejections:

      Rejections can only occur, when there is no license available anymore at the moment of request.

      If there are rejections, then the amount of Floating licenses should be increased.

    • Activity per host

      Similar analysis objective as with "Activity per user". Interesting when there are users with variable workplaces.

      License pulls:

      Single events of license pulls are counted.

      Shares:

      Single events of license releases are counted.

      Rejections:

      Rejections can only occur, when there is no license available anymore at the moment of request.

      If there are rejections, then the amount of Floating licenses should be increased.

    • Rejections by product

      Rejections:

      Rejections can only occur, when there is no license available anymore at the moment of request.

      Rejections show that the amount of Floating licenses should be increased.

    • Rejections by user

      Rejections:

      Rejections can only occur, when there is no license available anymore at the moment of request.

      Rejections show that the amount of Floating licenses should be increased.

    • Rejections by computer

      Rejections:

      Rejections can only occur, when there is no license available anymore at the moment of request.

      Rejections show that the amount of Floating licenses should be increased.

    • Usage by product

      How many different users and/or computers use which product?

      Is the number of computers higher than the number of users? This would show that there are users with variable workplaces.

      Number of computers:

      Number of users:

  • Show legend

    An additional legend is displayed (also in print).

  • Show as line graph:

    The depiction is changed from bar graph to line graph.

  • Columns

    Depending on the chosen statistic the respective columns are displayed.

    Hide not needed columns by clearing the checkbox.

  • Restrict

    Here you can filter with: Start date, End date, Products, User, Computer

    In the list fields select the desired values. At Products, User, Computer you can select any number of values via checkboxes.

    After changes please click on the button Update.

  • Diagram | Table view

    Right beside the setting options diagram and table view are displayed.

  • Buttons

    • Print:

      Print the result of the statistic evaluation.

      [Note] Note

      If the option Show legend is active, then the legend is used for printing as well.

      Print preview

      Print preview

    • Export data...:

      Export the data of statistic evaluation in a CSV file. In this way you can process the data in other programs.

      "Zeilenkopf","Abweisungen"
      "PSVBSCUSTO-IN-SW-IN-1F",18
      "PSDEVCUST-_ALL-SW-WI-1F",3
      "PSPROF-STL-SW-WI-1D",3
      "PDSTD-_ALL-SW-WI-1F",2
      "ECATDEVPRT-_ALL-SW-WI-1F",1
      "PSGEO-CAT4-SW-UX-1D",1