powered by CADENAS

Manual

Manual

4.16.3.5.4. No correlation to the old dataset found

If in an update version a directory, project or certain characteristic is missing, then it can be the case that LinkDB links have no target.

The Update manager signalizes this by a red cross in the index tree. The cross overlays the respective base symbol (directory , project , line ).

Example: Project and so logically also the lines do not exist anymore: Missing assignment not confirmed yet

Example: Project and so logically also the lines do not exist anymore: Missing assignment not confirmed yet

As soon as a certain characteristic is selected in the index tree, you can recognize on the right side, in the section Line mapping as well that there is no assignment:

  • Under Assigned project (New project) there is no entry

  • In the column New dataset there are no entries

  • No table is displayed

A missing automatic assignment of a project does not necessarily mean, that it does not exist; it could be that only the name has been changed.

For editing of assignments you have two options:

  1. Confirm missing assignment

    You can confirm the missing assignment now in the section Line mapping in the column New dataset via click on the green checkmark .

    In the directory structure, in the respective line the original symbol , marking a not available dataset, is overlapped with the green checkmark.

    -> In the LinkDB the link for the new dataset is deleted.

    Example: Project and so logically also the lines do not exist anymore: Missing assignment approved for a certain line

    Example: Project and so logically also the lines do not exist anymore: Missing assignment approved for a certain line

  2. Assign new line manually

    Now there are two further cases:

    • A new line assignment shall be made in the same project.

      -> Hereto change the line selection in the table and confirm with the command Approve assignment.

    • A new line assignment shall be made in another project.

      By clicking on the button Search project the dialog box Search opens on the tabbed page Search.

      Perform a text or variable search.

      [Note] Note

      The designation of the old dataset is already entered under Keyword. Of course you can also search with any other keyword.

      By double-clicking on one of the search results the desired part is assigned.

      Alternatively you can switch to the Choose tabbed page and there browse to the desired part/project. Then you can load the project via double-click into the column New dataset. Now select the desired characteristic.

      Regardless of the chosen variant now finally confirm the new assignment by clicking on the green checkmark Approve assignment.

      Now the symbol for an assigned and approved dataset is displayed in the index tree, in the respective line.