Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
2.3.3.
CoCreate Modeling Integration - Administration
2.3.3.7. Modelmanager -
Configuration
|
|
---|---|
Prev | Next |
In the following the most important settings are explained, which possibly can be adjusted:
With "true" the ModelManager is activated.
[PLM] ACTIVE_CONDITION=true
In which Modelmanager class the PARTsolutions parts are stored?
[CreationOptions] MM_ClassName(is3d)=LIBRARY_3D
In which Modelmanager class the PARTsolutions NativeCheckin parts are stored?
[CreationOptions] MM_ClassName(isNat)=MODEL_3D
For the attribute mapping there are two different attributes available:
Here in the example you can recognize it by the strings „MASTERDATA“ and „LIBRARY_3D“.
Attribute mapping is disabled by default.
[AttributeMapping(is3d)] ;Attr_Content_01(is3dPart)=ModelManagerAttributesPart ;Attr_Content_01(is3dAsm)=ModelManagerAttributesAsm ;Attr_Custom_01(is3dPart)="PSOL_PART" :class-name "LIBRARY_3D" :attachment :contents :allowed-owner-types :part-assembly ;Attr_Custom_01(is3dAsm)="PSOL_ASM" :class-name "LIBRARY_3D" :attachment :contents :allowed-owner-types :part-assembly ;Attr_Section_01=MODELMANAGERATTR ;Attr_Content_02=MODELMANAGERATTRMASTER ;Attr_Custom_02="PSOL_MASTER" :class-name "MASTERDATA" :attachment :contents :allowed-owner-types :part-assembly ;Attr_Section_02=MODELMANAGERATTR [MODELMANAGERATTR] ;Parts ;Assemblies [MODELMANAGERATTRMASTER] ;Master Data