powered by CADENAS

Manual

Manual

4.10.1.  material_assign.cfg (with ERP integration)

In the configuration file material_assign.cfg you can set which materials should be displayed in PARTdataManager, in the dialog box new ident-no..

During the export to the CAD system the PARTsolutions material is mapped onto the CAD system material so that the physical properties can be calculated in the CAD system.

More information

Information on the transfer of the material attribute to the CAD system can be found under Section 2.2.5, “Material mapping ”.

Information on the inclusion of the material into the file name can be found under Section 2.2.2.2, “File name: set generation options ("FileName" key) ”. Default: If a material information is available, include it into the file name.