Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Activate/deactivate the desired ports via checkbox. HTTP port and Service port are the standard ports without SSL encryption. Use HTTPS-Port and SSL-Service-Port if you want SSL encryption (normally either/or).
HTTPS-Port: 9022 (default): When activating the dialog area "SSL" is activated. See Section 4.5.6.3, “SSL encryption ”.
SSL-Service-Port: 9023 (default): When activating the dialog area "SSL" is activated. See Section 4.5.6.3, “SSL encryption ”.
You can display information on PARTapplicationServer here on the server or on the client as well. See Section 4.5.7, “ PARTapplicationServer Watch”.
Configuration file for the AppServer Server configuration
The
configuration file for the AppServer server configuration can be found
under $CADENAS_SETUP/pappserver.cfg
.
Normally the settings don't have to be changed.
Information on the individual keys are found in the configuration file itself.