powered by CADENAS

Manual

Manual

1.7.5.19.1.2.  Key "ExportSubAssemblyStructure" - Support for subassemblies

You can also transfer the subassembly structure to the CAD system

On this in the configuration file under $CADENAS_SETUP/partsol.cfg -> Key ExportSubAssemblyStructure set the value on "true".

$CADENAS_SETUP/partsol.cfg

[COMMON]
ExportSubAssemblyStructure=true

The feature is available for all CAD interfaces.

The following figure shows an assembly with subassembly in PARTdataManager.

Assembly with subassembly in PARTdataManager

Assembly with subassembly in PARTdataManager

The following two figures show the assembly structure (exemplarily in Solidworks) once with and once without subassembly.

Assembly without subassembly

Assembly without subassembly

Assembly with subassembly

Assembly with subassembly