powered by CADENAS

Manual

Manual

4.25.4.3.1.4.  Editing additional tables in the PARTlinkManager

In the PARTlinkManager you have the option not only to edit the ERPTABLE and LINKTABLE, but also edit any number of other tables within the LINKDB.

To do so, follow these steps:

  1. Indicate the tables to be changed in the file %CADENAS_SETUP%/plinkcommon.cfg under the section ADDITIONALTABLES.

    [ADDITIONALTABLES]
    #:VALS_S
    #:HELP;default;this table is used to store references concerning PLM-systems
    t0=PLMTABLE
    #:VALS_S
    #:HELP;default;this table is used to store Assembly-structures with 
      ERP-information
    t1=DATATABLE
    #:HELP;default;this table is used to store project-specific data 
      (ie. project specific partnames for CAD-files)
    t2=PLMTABLE2

    Add the key "t" followed by a continuously increasing number. As the value for the key, enter the database table.

    t1=DATATABLE

    t2=PLMTABLE2

    etc.

  2. Start the PARTlinkManagerconnect to the database (File -> Connect).

  3. Select the following: Extras -> Database -> Edit additional tables.

  4. Choose the desired table in the selection list under Select table.

    --> The table is displayed in the right half of the window and can now be edited.