Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Please perform the AppServer Client configuration in PARTadmin -> category AppServer client.[63]
Here, you can define how clients should access the AppServer, meaning via which ports, whether a local AppServer should be used, whether the AppServer has only to be used for searching or for catalog browsing as well.
The following listing explains the settings in detail:
Catalog browsing, search and database with AppServer and Catalog browsing and search with AppServer
There is only ONE central data directory for multi-installations.
All access (catalog browsing and search [at option Catalog browsing, search and database with AppServer to LinkDB as well]) is processed via PARTapplicationServer - regardless from which location.
Thus select one of these options, if PARTsolutions is used remotely without synchronization of catalog data.
|
|
Using the
local AppServer is advantageous compared to pdatamgr.exe
. This is
running on 64Bit, whereby possible memory problems are avoided.
The local AppServer is only used for searching, not for catalog browsing.
The AppServer is automatically started and exited together with PARTdataManager. If Seamless is also started, then Seamless uses the already running application.
Note | |
---|---|
More details on settings can be found under Section 4.5.8, “Set up ERP on PARTapplicationServer ”. |
Enter server address and ports: (only enabled when using one of the following options: Catalog browsing, search and database with AppServer | Catalog browsing and search with AppServer | Search with AppServer)
Activate/deactivate the desired ports via checkbox. HTTP port and Service port are the standard ports without SSL encryption. If SSL encryption is desired then use HTTPS-Port and SSL-Service-Port (normally either/or).
HTTPS-Port: 9022 (default): When activating the dialog area SSL is activated. See Section 4.5.6.3, “SSL encryption ”.
SSL-Service-Port: 9023 (default): When activating the dialog area SSL is activated. See Section 4.5.6.3, “SSL encryption ”.
Activate this option if you want SSL encryption. See Section 4.5.6.3, “SSL encryption ”.
Tunnel services via web sockets:
Optionally for SSL encryption. See Section 4.5.6.3, “SSL encryption ”.
If the AppServer is active, in PARTdataManager, down right in the status bar, a respective icon is displayed. The tooltip shows the respective information at mouseover.
There are five categories, which can be displayed at mouseover:
Which of the categories is displayed depends on the option chosen in PARTadmin -> category AppServer client -> AppServer connection.
With connection is displayed, otherwise .
[63] The
configuration file for the AppServer client configuration is found
under $CADENAS_SETUP/pappclient.cfg
.