Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Ein-/ausschalten des Synchronisierungs-Menü. Ausgeschaltet kann man per GUI die Vorberechnungsdatei nicht manuell aktualisieren.
Enable/disable the synchronization menu. If disabled the precalculation file cannot be updated per GUI manually. Default: false.
Block PARTconnection -> key ShowSynchronizationMenu -> value 0/1
The button is hidden, because manual update of the precalculation file is either not necessary or makes no sense.
At the first call up of the function Connection all required connection elements are indexed. You can recognize this at the progress bar.
After a catalog update the precalculation file is automatically updated.
After new ERP assignments the update should be started via script. See Section 1.10.2.1, “Connections ”.