Values
of all value range variables with names of the variables
CHANGEABLEVALUES
Values
of all value range variables that can be changed by user, in other
words are not locked (see common.cfg - LockDimRange=0/1)
CHANGEABLEVALUESWITHNAME
Changeable value range with name
CATALOG_NAME
Name of catalog
CATALOG_DESC
Visible
name of catalog (in current language)
SHORTNB
Short
standard description
CADSYSTEMNAME
Name of registered CAD system (if more than one
is registered, separate by comma)
CALCED_ROW
Row
number currently being calculated
NB
Standard name
LINA
BOM name
NENN
For DIN
912 z.B. $d.x$L. (only for standard parts, not catalogs)
NORM_NUMBER
Standard
number of a part
Located in the tab file; can be seen in
PARTeditor -> Identification specifications or in index
tree
NORM_TITLE
Standard title
of a part
Located in the
tab file; can be seen in PARTeditor -> Identification
specifications or in index tree
MATERIAL_NAME
Material (internal name) from material
dialog during export (see PARTdataManager -> Extras -> Settings -> Register PARTdataManager
-> Choose material on export; may be turned on/off)
(Attention:
For ERP functionality content, additional column
needed)
MATERIAL_DESC
Description text for material
(Attention: For ERP functionality
content, additional column needed)
LISTOFCOLUMNS
Display of
list with variable values of current row. The format of the
display may be influenced.
Example:
$LISTOFCOLUMNS(COLTYPE=ALL;EXCLUDE=D,L;
VALUE=$VARNAME.=$VARVALUE.)
COLTYPE
ALL Alle Variablen
VISIBLE Alle sichtbaren VAriablen
ERP Alle ERP Variablen
EXCLUDE Liste von VAriablen, die nicht ausgegeben
werden sollen
INCLUDE Liste von Variablen, die zusätzlich
zu den durch COLTYPE spezifizierten Variablen
ausgegeben werden sollen
VALUE Gibt an, wie die Daten für eine Variabele
ausgegeben werden sollen
Dabei können die folgenden Platzhalter
verwendet werden
$VARNAME. Variablenname
$VARDESC. Variablenbeschreibung
$VALDESC. Wertebeschreibung
$VARVALUE. Wert