powered by CADENAS

Manual

Manual

1.1.6.6.12.2. Block [TopSearchPane]

1.1.6.6.12.2.1.  Keys "ShowFulltelocationxtSearch" "ShowFulltextSearchPathSelection" "ShowCatalogFilter" - Hide search fields [TopSearchPane]

See also:

[Note] Note

If whether block nor key are available, apply these yourself.

The values can be set to 0 (off) or 1 (on).

In the TopSearchPane block you can hide the search fields in the PARTdataManager Project selection area. (Possibly required for the offline CD).

  • ShowFulltelocationxtSearch=0/1

    If this value is set to 0, then the complete upper row Keyword search is hidden.

  • ShowFulltextSearchPathSelection=0/1

    If this value is set to 0, then only the list field for the path selection is hidden.

  • ShowCatalogFilter=0/1

    If this value is set to 0, then the complete lower row Catalog filter is hidden.

1.1.6.6.12.2.1.1. Block: [DidYouMeanSearch] -
1.1.6.6.12.2.1.1.1.  Key "Enabled" - an/aus

Show/hide the feature "Did you mean":

Key: Enabled

Value: 0/1

Did you mean

Did you mean

1.1.6.6.12.2.1.1.2. Key "ShowInBalloon" - "Did you mean" tooltip on/off

Show/hide tooltip

Key: ShowInBalloon

Value: yes/no

1.1.6.6.12.2.1.2. Block [SimilarWordsSearch]

[SimilarWordsSearch]

Show/hide

Enabled=0/1

Modify search with related terms

Modify search with related terms