Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
5.9. Configure
new ident-no. dialog box
5.9.4.
Automatically generated
ERP_PDM_NUMBER at new creation of parts (on/off) - erpcustom.cfg -> Block
[VARS] -> Key "TIMESTAMPNR"
|
|
---|---|
Prev | Next |
In PARTdataManager, when clicking on Add dataset to link database , the dialog box new ident-no. opens.
You can configure whether the ERP number should be manually inserted or automatically generated as "Timestamp" number. For automatic generation the input field is displayed inactively (dimmed).
Setting per configuration file
erpcustom.cfg -> Block [VARS] -> Key "TIMESTAMPNR"
Value range of key TIMESTAMPNR: 0/1
In PARTadmin, in the category
Configuration files, under CADENAS_SETUP
, open the
configuration file erpcustom.cfg
.
In the block VARS, change the default entry in TIMESTAMPNR from '0' to'1'.
Example with activated key TIMESTAMPNR:
Select a part which doesn't have a number yet.
Click on the button Add dataset to link database .
Please regard: The input field ERPNo is enabled, because the ERP number is automatically generated.
The ERP number is inserted with automatically generated ERP number.