powered by CADENAS

Manual

Manual

5.9.5.1.2. Activating ERP Number Generator

Before you can use the ERP Number Generator you must make the appropriate settings in PARTadmin.

In PARTadmin, under CADENAS_SETUP open the configuration file erpcustom.cfg in the dialog area Category.

Set the settings as follows:

  • TIMESTAMPNR=0

  • ERPNR_ENABLED=0 (Activate the key - if needed - per right-click on the key name)

  • erp_nrgenerator (Activate the key per right-click on the key name)

Save changes.

Now both keys ERP_NRGENERATOR and ERP_NRGENERATOR_CONDITIONS are used.

With both these keys you define the pattern after which the ERP numbers are to be generated.