powered by CADENAS

Manual

Manual

3.3.12.3. Installation

[Note] Note

Prerequisite for the installation of Windchill PDMLink is that the CAD interface is installed properly.

In addition, a connection to the server must be present as well.

Do the following:

  • Open Tools -> Server registration in ProE.

    -> The server registration dialog shows up in which one can select the server and set up the library.

    Server registration

    Server registration

  • Choose Server -> Register new server.

    Under Name enter a name for the server. Under Storage location the IP address of the server is entered. Here it is important to set /Windchill after the server name. Only then will a server be found.

    Server registration

    Server registration

    Register new server

    Register new server

    If you click on Check the existing library is searched through. It is then displayed in the lower window. If you are searching for the correct library and then click on OK, the workspace will now use this library as the workspace of the user in ProE.