powered by CADENAS

Manual

Manual

1.1.1.1. Client authorization rights

Pay attention that no administration modules like PARTlinkManager or PARTadmin are installed on user clients or restrict access via Windows authorization rights!

PARTadmin started without administration rights

  • In some categories the authorization rights are mandatory.

    [Note] Note

    Accessing files under $CADENAS_USER is possible without administrative authorization rights.

    Thus language settings can be performed without administrative authorization rights.

    Missing rights are identified by the lock icon.

  • If the information symbol is shown in the toolbar, this means that PARTadmin was not started in administrative mode. By clicking on the icon, PARTadmin is restarted - this time with Admin rights.

    [Note] Note

    The icon is only displayed when the UAC-Modus is activated.

Restricted authorization rights

Restricted authorization rights