powered by CADENAS

Manual

Manual

1.1.3.4.2. Overview of user interface

The following figure shows the user interface of PARTadmin.

PARTadmin -> Category: Index administration

PARTadmin -> Category: Index administration

The PARTadmin user interface when selecting Index administration is divided into the following areas:

  1. Menu and toolbar

  2. Category selection

    All administration operations are carried out within PARTadmin.

    Via Category, select the specific application (z.B. Index administration, Catalog update or ERP environment)

    The current section contains information about Index administration.

    [Note] Note

    Areas 1 and 2 remain the same for all PARTadmin functions.

  3. Index administration page

    • Commands

    • Legend

      Additional detailed information concerning full-text search index is found under Section 1.1.3.4.5.2.1, “Matrix: Software and Lucene index version”.

    • Tree with main directories

      • Catalogs

        All installed catalogs are displayed here.

      • My Parts

        The following own parts are managed/displayed here:

      • Classifications

        All installed classifications are managed here.

      • User data

        In the index tree, under User data, the Favorites and History are managed.

        • Favorites

          All favorites set in the PARTdataManager are displayed here.

          You can also hide certain displays of different directories in the PARTdataManager.

        • History

          The complete history of the parts used in the PARTdataManager are displayed here.

          You can also hide certain displays of different directories in the PARTdataManager.

      • Fingerprints

        This category is only used by vbs scripts. It is especially available for compatibility to V8.1 reasons, in order to also have the option to search geometrically without the part being available in V9.

    • Preview images

      Preview images of directories and projects are displayed at the right.

  4. Progress display of the Index update

    [Note] Note

    The area 4 Index update can be activated in the context menu of the title bar, the menu or the toolbar.

    Index update

    Index update

  5. Messages

    Errors are displayed in the Messages window.

  6. Index accessible / locked

    In the status bar, an icon shows whether the index is locked.

    If a green lock icon is displayed then PARTadmin can access the index.

    If a red lock icon is displayed then the index is locked.

    When moving the mouse over the icon a tooltip is displayed where you can see which computer and which application is responsible.