Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
5.11.1.
Tabbed
page "General"
5.11.1.1. Dialog box for
role selection - plinkgroups.cfg -> Block [Role name] -> Keys "DESC"
and "IMAGE"
|
|
---|---|
Prev | Next |
Note | |
---|---|
The setting for the Select role dialog box is role dependent, so has to be defined for each role separately. |
You can specify an image and a description.
If several roles are available for a user, the dialog box Select role opens when starting the application. Furthermore it can be called anytime via button Select group .
Setting in
configuration
file $CADENAS_SETUP/plinkgroups.cfg
:
Block [<role name>], key DESC, value contains description text; key IMAGE, value contains image path
[DEPARTMENT1] ... DESC=Department1 ... IMAGE=$(CADENAS_SETUP)/bitmaps/linkdbdemo/department/department1.bmp ...
Setting in user interface under PARTadmin -> category Roles -> tabbed page General -> Description and Displayed bitmap
Tip | |
---|---|
Just specify a simple placeholder under "Description". It can be translated into the desired languages. |
Determine sorting sequence of roles in the dialog box